This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

New warning on ARM 16.3.0.STS

Hey guys,

with the TI ARM toolchain version 16.3.0.STS, the intrinsics for enabling/disabling interrupts have been optimized. This causes a new warning when compiling in Thumb mode:

"C:\Users\mike\AppData\Local\Temp\0970010", WARNING! at line 514: [W0004]
         Missing condition code inside of IT block
                CPSIE     i                     ; [DPU_4_PIPE0] |1538|

Please investigate and give feedback.

Regards,
Michael 

  • This does appear to be a bug in the tools.  Please submit a test case to help us determine the cause and find a fix.  We need the preprocessed source file which causes this problem.  We also need to see the build options exactly as the compiler sees them.

    Thanks and regards,

    -George

  • Here you are

    ;* --------------------------------------------------------------------------*
    ||$C$L23||:    
            ADD       SP, SP, #28           ; [DPU_4_PIPE0] 
            POP       {V1, V2, V3, V4, V5, V6, PC} ; [DPU_4_PIPE1] 
            ; BRANCH OCCURS                  ; [] 
    	.sect	".IO_DRIVER_CODE:IO_MPU_Enable"
    	.align	16
    	.clink
    	.thumbfunc IO_MPU_Enable
    	.thumb
    	.asg	"no_stm_memcpy", memcpy
    	.asg	"no_stm_memset", memset
    	.global	IO_MPU_Enable
    
    ;*****************************************************************************
    ;* FUNCTION NAME: IO_MPU_Enable                                              *
    ;*                                                                           *
    ;*   Regs Modified     : A1,A2,A3,A4,V1,V2,V3,V9,SP,LR,SR,D0,D0_hi,D1,D1_hi, *
    ;*                           D2,D2_hi,D3,D3_hi,D4,D4_hi,D5,D5_hi,D6,D6_hi,D7,*
    ;*                           D7_hi,FPEXC,FPSCR                               *
    ;*   Regs Used         : A1,A2,A3,A4,V1,V2,V3,V9,SP,LR,SR,D0,D0_hi,D1,D1_hi, *
    ;*                           D2,D2_hi,D3,D3_hi,D4,D4_hi,D5,D5_hi,D6,D6_hi,D7,*
    ;*                           D7_hi,FPEXC,FPSCR                               *
    ;*   Local Frame Size  : 0 Args + 0 Auto + 16 Save = 16 byte                 *
    ;*****************************************************************************
    IO_MPU_Enable:
    ;* --------------------------------------------------------------------------*
    ;** 504	-----------------------    if ( region_id < 4u ) goto g3;
    ;** 554	-----------------------    return 31;
            CMP       A1, #4                ; [DPU_4_PIPE0] |504| 
            STR       LR, [SP, #-4]!        ; []  PUSH {V1, V2, V3, LR} ; [DPU_4_PIPE0] 
            STR       V3, [SP, #-4]!        ; []  PUSH {V1, V2, V3, LR} ; [DPU_4_PIPE0] 
            STR       V2, [SP, #-4]!        ; []  PUSH {V1, V2, V3, LR} ; [DPU_4_PIPE0] 
            STR       V1, [SP, #-4]!        ; []  PUSH {V1, V2, V3, LR} ; [DPU_4_PIPE0] 
            IT        CS                    ; [] 
            MOVCS     A1, #31               ; [DPU_4_PIPE0] |554| 
            MOVW      A2, IO_MPU_regionInitialized+0 ; [DPU_4_PIPE0] |507| 
            BCS       ||$C$L24||            ; [DPU_4_PIPE1] |554| 
            ; BRANCHCC OCCURS {||$C$L24||}   ; [] |554| 
    ;* --------------------------------------------------------------------------*
    ;**	-----------------------g3:
    ;** 507	-----------------------    if ( IO_MPU_regionInitialized[region_id] ) goto g5;
    ;** 554	-----------------------    return 33;
            MOVT      A2, IO_MPU_regionInitialized+0 ; [DPU_4_PIPE0] |507| 
            LDRB      A2, [A2, +A1]         ; [DPU_4_PIPE0] |507| 
            CMP       A2, #0                ; [DPU_4_PIPE0] |507| 
            IT        EQ                    ; [] 
            MOVEQ     A1, #33               ; [DPU_4_PIPE0] |554| 
            MOVW      A3, IO_MPU_regionEnabled+0 ; [DPU_4_PIPE0] |511| 
            BEQ       ||$C$L24||            ; [DPU_4_PIPE1] |554| 
            ; BRANCHCC OCCURS {||$C$L24||}   ; [] |554| 
    ;* --------------------------------------------------------------------------*
    ;**	-----------------------g5:
    ;** 511	-----------------------    K$15 = &IO_MPU_regionEnabled[region_id];
    ;** 511	-----------------------    if ( !*K$15 ) goto g7;
    ;** 554	-----------------------    return 330;
            MOVT      A3, IO_MPU_regionEnabled+0 ; [DPU_4_PIPE0] |511| 
            ADDS      A3, A3, A1            ; [DPU_4_PIPE0] |511| 
            LDRB      A2, [A3, #0]          ; [DPU_4_PIPE0] |511| 
            CMP       A2, #0                ; [DPU_4_PIPE0] |511| 
            IT        NE                    ; [] 
            MOVNE     A1, #330              ; [DPU_4_PIPE0] |554| 
            BNE       ||$C$L24||            ; [DPU_4_PIPE1] |554| 
            ; BRANCHCC OCCURS {||$C$L24||}   ; [] |554| 
    ;* --------------------------------------------------------------------------*
    ;**	-----------------------g7:
    ;** 523	-----------------------    saved_cpsr = _disable_IRQ();
    ;** 526	-----------------------    saved_fiqs = *(C$1 = (volatile unsigned *)0xfffffe30u)&0xc00u;
    ;** 527	-----------------------    C$1[4] = 3072u;
    ;** 532	-----------------------    *K$15 = 1;
    ;** 535	-----------------------    _mpuSetRegion_(region_id+8u);
    ;** 535	-----------------------    mpu_status = _mpuGetRegionSizeAndEnable_();
    ;** 535	-----------------------    _mpuSetRegionSizeAndEnable_(mpu_status |= 1u);
    ;** 538	-----------------------    *C$1 = saved_fiqs;
    ;** 541	-----------------------    if ( saved_cpsr&0x80u ) goto g9;
            MRS       V2, CPSR              ; [DPU_4_PIPE0] |523| 
            CPSID     i                     ; [DPU_4_PIPE0] |523| 
            MOVW      V3, #65072            ; [DPU_4_PIPE0] |526| 
            MOVT      V3, #65535            ; [DPU_4_PIPE0] |526| 
            MOVS      A2, #1                ; [DPU_4_PIPE0] |532| 
            STRB      A2, [A3, #0]          ; [DPU_4_PIPE0] |532| 
            ADDS      A1, A1, #8            ; [DPU_4_PIPE1] |535| 
            LDR       V1, [V3, #0]          ; [DPU_4_PIPE0] |526| 
            MOV       A2, #3072             ; [DPU_4_PIPE1] |527| 
            STR       A2, [V3, #16]         ; [DPU_4_PIPE0] |527| 
            BL        _mpuSetRegion_        ; [DPU_4_PIPE1] |535| 
            ; CALL OCCURS {_mpuSetRegion_ }  ; [] |535| 
    ;* --------------------------------------------------------------------------*
    ;** 543	-----------------------    _enable_IRQ();
    ;**	-----------------------g9:
    ;** 554	-----------------------    return 0;
            BL        _mpuGetRegionSizeAndEnable_ ; [DPU_4_PIPE1] |535| 
            ; CALL OCCURS {_mpuGetRegionSizeAndEnable_ }  ; [] |535| 
            ORR       A1, A1, #1            ; [DPU_4_PIPE0] |535| 
            BL        _mpuSetRegionSizeAndEnable_ ; [DPU_4_PIPE1] |535| 
            ; CALL OCCURS {_mpuSetRegionSizeAndEnable_ }  ; [] |535| 
            AND       V1, V1, #3072         ; [DPU_4_PIPE0] |526| 
            STR       V1, [V3, #0]          ; [DPU_4_PIPE0] |538| 
            LSRS      A1, V2, #8            ; [DPU_4_PIPE1] |541| 
            IT        CC                    ; [] 
            CPSIE     i                     ; [DPU_4_PIPE0] |543| 
            MOVS      A1, #0                ; [DPU_4_PIPE0] |554| 
    ;* --------------------------------------------------------------------------*

    C_OPTS      :=  -mv7R4                         \
                    --abi=eabi                     \
                    --auto_inline=0                \
                    --endian=big                   \
                    --float_support=VFPv3D16       \
                    --plain_char=unsigned          \
                    --small_enum                   \
                    --fp_mode=strict               \
                    --opt_level=2                  \
                    --opt_for_speed=3              \
                    --code_state=16                \
                    --no_inlining                  \
                    --gen_func_subsections         \
                    --check_misra=none             \
                    --issue_remarks                \
                    --display_error_number         \
                    --quiet                        \
                    --aliased_variables            \
                    --no_stm                       \
                    --unaligned_access=off

  • Thank you for showing the build options.  The file you attached is not the one needed.  It shows the assembly output of the compiler.  I need the C source which the compiler processes to generate the problem assembly.

    Thanks and regards,

    -George

  • George,

    I see. Unfortunately I cannot post the output of this pp file here as it would unveil huge pieces of our production code.

    So I came up with an alternative. This minimal code piece is perfectly suitable to reproduce the problem:

    void testfunction (void)
    {
        unsigned int saved_cpsr;
    
        /* save and disable IRQs locally */
        saved_cpsr = (unsigned int)_disable_IRQ();
      
        /* do some critical section handling here */
        
        /* restore IRQs */
        if ((saved_cpsr & 0x00000080UL) == 0U)
        {
            (void)_enable_IRQ();
        }
    }

    Regards,
    Michael

  • Thank you for the test case.  I can reproduce the problem.  I filed SDSCM00052849 in the SDOWP system to have this investigated.  You are welcome to follow it with the SDOWP link below in my signature.

    Thanks and regards,

    -George