Other Parts Discussed in Thread: SYSBIOS
Team,
I am using TI CGT C6000 8.1.0. I m compiling a complex stack that previously compiled fine for ARM (gcc). Now I get internal errors on two files, both issues seem to be related to complex struct defines. The actual instructions at the logged lines are trivial:
e.g.:
stWriteRsp.ARUUID = AREP_GET_ARUUID(lpArep);
now the struct fr stWriteRsp is this:
struct _ST_IOD_READ_WRITE
{
APP_WORD Seq_Number;
ST_CLR_RPC_UUID ARUUID;
ALIGNED_DWORD_DECL(API);
APP_WORD Slot_Number;
APP_WORD Subslot_Number;
APP_WORD Padding;
APP_WORD Index;
ALIGNED_DWORD_DECL(Record_Data_Length);
union {
struct {
APP_BYTE RWPAdding[RW_PADDING_LEN];
}Wr_Req;
struct {
APP_WORD AddData1;
APP_WORD AddData2;
APP_BYTE ErrorCode;
APP_BYTE ErrorDecode;
APP_BYTE ErrorCode1;
APP_BYTE ErrorCode2;
}Wr_Res;
}RdWr_u;
}STRUCT_ALIGNEMENT;
typedef struct _ST_IOD_READ_WRITE PACK_ALIGNEMENT(ST_IOD_READ_WRITE), APP_FAR * LPST_IOD_READ_WRITE;
followed by the struct for ARUUID:
struct _ST_CLR_RPC_UUID {
ALIGNED_DWORD_DECL(Data1); /*4 - 0*/
APP_WORD Data2; /*2 - 4*/
APP_WORD Data3; /*2 - 6*/
APP_BYTE Data4[UUID4LEN]; /*8 - 8*/
}STRUCT_ALIGNEMENT; /* 16*/
typedef struct _ST_CLR_RPC_UUID PACK_ALIGNEMENT(ST_CLR_RPC_UUID), APP_FAR* LPST_CLR_RPC_UUID;
As you can see it won't be trivial to reproduce without providing full sources... however this is a 3P stack with a lot of dependencies to our IA-SDK...
Unfortunately the issue is time critical as we need to deliver a project based on this to a large customer by end of the week!
Is there a compiler expert that would walk with me through the code by webex to find a workaround? I know that is a stretch but I don't know what else to do here. Any tips welcome...
Best regards,
Frank
Here is the log:
**** Build of configuration Debug for project Nimu_ICSS_idkAM572x_c66x ****
"C:\\TI\\ccs613\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.c'
'Invoking: C6000 Compiler'
"C:/TI/ccs613/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0/bin/cl6x" -mv6600 --include_path="C:/TI/ccs613/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/protocols/snmp/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/src/addin/mrp/mrc_only" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include/mrp" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/pndeviceSysBios" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/src/addin/mrp" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/protocols/profinet_slave/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include/os_SYSBIOS" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/include/RT_MRP" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x" -g --define=SOC_AM572x --define=AM57XX_FAMILY_BUILD --define=IDK_AM572X --define=USE_BIOS --define=C66X --define=NSS_GEN2 --diag_warning=225 --diag_warning=994 --diag_warning=262 --diag_wrap=off --diag_suppress=1111 --diag_suppress=827 --diag_suppress=824 --diag_suppress=837 --diag_suppress=1037 --diag_suppress=195 --diag_suppress=77 --diag_suppress=232 --display_error_number --preproc_with_compile --preproc_dependency="third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.d" --obj_directory="third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc" --cmd_file="configPkg/compiler.opt" "../third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.c"
>> Compilation failure
third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/subdir_rules.mk:21: recipe for target 'third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.obj' failed
"C:\TI\industrial-automation-lab\Projects\PN_AM57x_DSP\NimuICSS_idkAM572x_c66x\third_party\protocols\profinet_slave\IO-Device\src\addin\mrp\mrp_datatypes.h", line 47: warning #303-D: typedef name has already been declared (with same type)
>> ../third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.c, line 426:
INTERNAL ERROR: Decomposition error
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
gmake: *** [third_party/protocols/profinet_slave/IO-Device/src/toolkit/msg_acyc/frmgendv.obj] Error 1
'Building file: ../third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.c'
'Invoking: C6000 Compiler'
"C:/TI/ccs613/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0/bin/cl6x" -mv6600 --include_path="C:/TI/ccs613/ccsv6/tools/compiler/ti-cgt-c6000_8.1.0/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/protocols/snmp/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/src/addin/mrp/mrc_only" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include/mrp" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/pndeviceSysBios" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/src/addin/mrp" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/protocols/profinet_slave/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include/os_SYSBIOS" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/include/RT_MRP" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x/third_party/protocols/profinet_slave/IO-Device/include" --include_path="C:/TI/industrial-automation-lab/Projects/PN_AM57x_DSP/NimuICSS_idkAM572x_c66x" -g --define=SOC_AM572x --define=AM57XX_FAMILY_BUILD --define=IDK_AM572X --define=USE_BIOS --define=C66X --define=NSS_GEN2 --diag_warning=225 --diag_warning=994 --diag_warning=262 --diag_wrap=off --diag_suppress=1111 --diag_suppress=827 --diag_suppress=824 --diag_suppress=837 --diag_suppress=1037 --diag_suppress=195 --diag_suppress=77 --diag_suppress=232 --display_error_number --preproc_with_compile --preproc_dependency="third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.d" --obj_directory="third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl" --cmd_file="configPkg/compiler.opt" "../third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.c"
>> Compilation failure
third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/subdir_rules.mk:14: recipe for target 'third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.obj' failed
"C:\TI\industrial-automation-lab\Projects\PN_AM57x_DSP\NimuICSS_idkAM572x_c66x\third_party\protocols\profinet_slave\IO-Device\src\addin\mrp\mrp_datatypes.h", line 47: warning #303-D: typedef name has already been declared (with same type)
>> ../third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.c, line 296:
INTERNAL ERROR: Decomposition error
This may be a serious problem. Please contact customer support with a
description of this problem and a sample of the source files that caused this
INTERNAL ERROR message to appear.
Cannot continue compilation - ABORTING!
gmake: *** [third_party/protocols/profinet_slave/IO-Device/src/toolkit/sttup/aseimpl/plugsm.obj] Error 1
gmake: Target 'all' not remade because of errors.