Following code compiles fine with 5.2.x and throws a warning on 15.12.3 and 16.x
.sect ".text_krn"
.thumb
.thumbfunc hello
hello:
movs r0,#-0xffffffff
.end
Why this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you for reporting this problem, and supplying a well defined test case. I can reproduce the problem. I filed CODEGEN-1547 in the SDOWP system to have this investigated. You are welcome to follow it with the SDOWP link below in my signature.
Thanks and regards,
-George
42Bastian said:the SDOWP lists only 15.12.3.LTS, but 16.6.0.STS contains the same bug.
I updated the record.
Thanks and regards,
-George