This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Bug: MISRA-C Rule 7.1 Misreported by arm compiler



Code:

static int k_02;

#define INC_K(num) k_##num++; 

void test(int i) {
    INC_K(02);
}

Command line:

C:/ti/ccsv6/tools/compiler/arm_15.12.3.LTS/bin/armcl -mv7R4 --code_state=32 --float_support=VFPv3D16 -O4  --check_misra="7.1" -g --strict_ansi --emit_warnings_as_errors --diag_wrap=off --diag_warning=225 --display_error_number --abi=eabi --enum_type=packed --preproc_with_compile misra_7_1.c

Output:

"misra_7_1.c", line 6: error #1382: (MISRA-C:2004 7.1/R) Octal constants (other than zero) and octal escape sequences shall not be used
1 error detected in the compilation of "misra_7_1.c".

IMHO in this case "02" isn't constant, this is macro parameter.