This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not able to compile assembly file with latest compiler for c55X 'cl55.exe'

Hi Recently , I downloaded CGT 4.4.1 for c55x & i am not bale to compile my assembly file . 

The error shown is  

 ERROR! at line 327: [E0800]        Cannot apply a D-unit conditional execute instruction to an Smem read-modify-write that is lock()'d .

Error Line  :  BSET T1, *AR1

Previously I used old CGT  version 2.2  in which the compilation is successful.

Command used : cl55.exe -c <filenamecopy_data.asm>

Kindly help in solving this issue with the latest compiler.

Attached the asm File . 

Also find the stack dump produced by compiler while compiling (cl55.exe.stackdump)

Exception: STATUS_ACCESS_VIOLATION at eip=610C8439

eax=00000000 ebx=00000001 ecx=00000000 edx=0000016C esi=00000000 edi=1AACCCB0
ebp=1AACCAEC esp=1AACCAC4 program=\\?\D:\development\parallelbuild\legacy_mcl\tools\C5500\cgtools_4.4.1\bin\cl55.exe, pid 3260, thread unknown (0x4790)
cs=0023 ds=002B es=002B fs=0053 gs=002B ss=002B
Stack trace:
Frame Function Args
1AACCAEC 610C8439 (00000000, 00000000, 00000000, 00000000)
1AACCBFC 610C8DD5 (00000000, 00000000, 00000000, 00000000)
1AACCCBC 610C9B3A (FFFFFFFF, FFFFFFFF, 75B145DF, FFFFFFFE)
1AACCD0C 61028182 (00000002, F60B4CFA, 1AACCE64, 00000002)
1AACCD98 755F7661 (00000002, 1AACCDD4, 755F74AC, 00000002)
End of stack trace

  • The newer compiler checks for silicon bugs which were unknown when the older compiler was released.  Thus you see ...

    Balaganesh V said:
     ERROR! at line 327: [E0800]        Cannot apply a D-unit conditional execute instruction to an Smem read-modify-write that is lock()'d .

    It is unlikely your device actually has this silicon bug.  Most such bugs are fixed in recent devices.  You can avoid unnecessary silicon bug checks by using -v to specify the device you use.  For example, this command ...

    C:\some\dir\path>cl55 -vOMAP2140 copy_data.asm

    ... builds clean.  Without -v, all silicon bugs are checked.  With -v, only the bugs relevant to that device are checked.  Use -vlist to see a list of all the device names recognized by -v.

    Balaganesh V said:
    Also find the stack dump produced by compiler while compiling (cl55.exe.stackdump)

    Do you experience this stack dump while building copy_data.asm?  I cannot reproduce that behavior.  Please submit the source file that causes the stack dump.  Also show all the build options exactly as the compiler sees them.

    Thanks and regards,

    -George

  • Hi George , 

    Thanks for the info . 

    My silicon version seems to be -v5510:2.2

    Here are the CFLAGS passed to the legacy compiler (V2.2.1) :  -pds232 -pds14 -qq -v5510:2.2 -mp -ml

    Now My job is to upgrade the tool chain . 

    I tried passing the same to the new compiler (v4.4.1) & faced the error. 

    Is there a way to suppress this error & get the file compiled. pls try from your side & share me the CFLAGS.

    Note : Iam unaware why -pds232 & -pds14 are passed . 

    Also the error displayed is like this ERROR!   at line 327: [E0800] . whether 800(decimal or hex) is the error number ? Whether we can suppress this . 

    I tried with new version of  masm55,exe also .

    Kindly share your info

    Note : The previous stack dump I have shared is not due to this copy_data.asm file . I will check regarding this  & share you later .

  • Balaganesh V said:
    Here are the CFLAGS passed to the legacy compiler (V2.2.1) :  -pds232 -pds14 -qq -v5510:2.2 -mp -ml

    I think it makes sense to explain the background for all of these options, so you can make an informed decision about how to handle them.

    With regard to -pds232 and -pds14 ...  This tells the compiler to suppress diagnostics with those ID numbers.  Which raises the question: What diagnostics correspond to those ID numbers?  You can look that up in this wiki article.  

    With regard to -qq ... This tells to the compiler to be super-quiet about progress messages issued to the console during a build.  All such progress messages are suppressed.  To see what you are missing, try -q instead, or remove it altogether.

    With regard to -v5510:2.2 ... This says to build for silicon device C5510 version 2.2.  I do not know how old that device is.  It is at least 10 years old, probably older.  It is very unlikely you use that device now.  You need to determine which device you use now, and change this option to match.  It is possible you use a device that is not recognized by the -v switch.  In that case, you need to determine the version of the CPU core in your device, and then supply the option -vcpu:version .  For example -vcpu:3.3.  I cannot help you determine the version of the CPU core in your C5500 device.  For that, I recommend you start a new thread in the C5000 device forum.  Once you begin using the correct -v option, it is likely that most of your problems will go away.

    With regard to -mp ... This is an undocumented option.  I cannot discuss it in a public forum like this.  It is very unlikely you need this option.  I'll contact you privately with further detail.  For other readers of this thread: I guarantee that you never need this option.

    With regard to -ml ... This means use large memory model.  It is replaced by the option --memory_model=large.

    Thanks and regards,

    -George

  • Hi George ,

    Thanks for the info . Yes ,Its a legacy product & using c5510 .
    From this link processors.wiki.ti.com/.../C55x_CPU_revision.pdf , Iam able to find the core & cpu version .
    It was -vcpu:2.1 or -vcore:2.1 . But file is not getting compiled even with these options .
    Could Please try once & share your view on this .
  • Thank you for your patience.  I think you have found a bug in the assembler.  It only occurs when building for that old CPU revision.  I filed CODEGEN-1731 in the SDOWP system.  Normally I'd say this bug will be addressed.  But the C5500 compiler tools are no longer under active development.  It is unlikely this bug will get fixed.  The purpose of filing the bug is to have the experts devise a workaround.  I'm pretty sure the workaround will require changing the assembly source.  

    Thanks and regards,

    -George

  • Thanks for your reply . 

    Kindly share the workaround . It will be very helpful to continue my work. 

    Thanks and Regards,

    Balaganesh.V

  • I'm sorry, this is an actual requirement for CPU rev 1 and 2. Prior to CPU rev 3, all RMW instructions have locking semantics, so the BSET instruction is in fact locked. For CPU rev 3, RMW instructions have locking semantics only when using the lock qualifier. (BSET.LK T1, *AR1). You should change the XCCPART instruction immediately preceding the BSET intruction into an XCC instruction.

    There was a bug (SDSCM00008387, not published) in the assembler because it did not emit this necessary error message until version 2.85.