Part Number: TDA3
Tool/software: TI C/C++ Compiler
Having installed TI ARM v17.6.0.STS into CCS 7.2.0.00013 running under Windows 10 pro 64-bit the automatic library build was failing. E.g.:
**** Build of configuration Debug for project TDA3x_Cortex_M_sadd16 **** "C:\\ti\\ccs720\\ccsv7\\utils\\bin\\gmake" -k -j 4 all -O 'Building target: TDA3x_Cortex_M_sadd16.out' 'Invoking: ARM Linker' "C:/ti/ccs720/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armcl" -mv7M4 -g --diag_warning=225 --diag_wrap=off --display_error_number -k -z -m"TDA3x_Cortex_M_sadd16.map" -i"C:/ti/ccs720/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/lib" -i"C:/ti/ccs720/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="TDA3x_Cortex_M_sadd16_linkInfo.xml" --rom_model --be32 -o "TDA3x_Cortex_M_sadd16.out" "./main.obj" -llibc.a <Linking> warning #10366-D: automatic library build: using library "C:\ti\ccs720\ccsv7\tools\compiler\ti-cgt-arm_17.6.0.STS\lib\rtsv7M4_T_be_v4SPD16_eabi.lib" for the first time, so it must be built. This may take a few minutes. process_begin: CreateProcess(NULL, echo Creating library c:/users/mr_hal~1/appdata/local/temp/ti9b5d~1/rtsv7m4_t_be_v4spd16_eabi.lib, ...) failed. Makefile:1948: recipe for target 'library' failed make (e=2): The system cannot find the file specified. >> Compilation failure makefile:140: recipe for target 'TDA3x_Cortex_M_sadd16.out' failed
I don't have make, gmake or sh from any other utility in the path. The automatic library build from TI ARM v17.3.0.STS was working.
The error message from the TI ARM v.17.6.0.STS automatic library build says gmake failed to execute the process with the command line "echo Creating library c:/users/mr_hal~1/appdata/local/temp/ti9b5d~1/rtsv7m4_t_be_v4spd16_eabi.lib".
Comparing the TI ARM v17.3.0.STS and v17.6.0.STS installations shows that in the lib\src\Makefile v17.6.0.STS has added an echo as part of the library target:
library: $(ALL_OBJS) @echo Creating library $(LIB) @$(CD) $(OBJ); $(AR) -qa $(LIB) $(notdir $(ALL_OBJS))
I think the unquoted string in causing gmake to abort the build with an error. As an experiment modified the v17.6.0.STS lib\src\Makefile to quote the echo string and the automatic library build was then successful:
library: $(ALL_OBJS) @echo "Creating library $(LIB)" @$(CD) $(OBJ); $(AR) -qa $(LIB) $(notdir $(ALL_OBJS))
Not sure if this is a bug in the v17.6.0.STS lib\src\Makefile or something about my PC setup, but at least allowed the automatic library build to complete successfully.