Part Number: TM4C1237H6PZ
Tool/software: TI C/C++ Compiler
Hi Support,
my customer is having some troubles with the linker in the version 16.9.4 LTS of the compiler.
Basically, it doesn't like the memory filling option in the linker command file stated by the following line
FLASH (RX) : origin = FLASH_START, length = START(CRCDATA)-FLASH_START, fill = 0xFFFFFFFF
If the filling option is removed, everything runs fine. Can you help me solving the issue?
This is the linking command displayed in the output console.
'Building target: 4555290_NCC.out'
'Invoking: ARM Linker'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.4.LTS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --define=ccs="ccs" --define=PART_TM4C1237H6PZ --define=TARGET_IS_BLIZZARD_RB1 --define=__STDC_LIMIT_MACROS --define=_32_BIT_DOUBLE --float_operations_allowed=32 --gcc --diag_suppress=10190 --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --check_misra="2.1,2.3,4,5.2,5.3,5.4,6.1,6.2,6.4,6.5,7,8.1,8.2,8.5,8.6,8.8,8.11,8.12,9" -z -m"4555290_NCC.map" --heap_size=2048 --stack_size=0 -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.4.LTS/lib" -i"C:/ti/TivaWare_C_Series-2.1.3.156/driverlib/ccs/Debug" -i"C:/Projects/BIC - 0580181 - Cosmogas/2 - Develop/5 - Firmware/4555290_NCC/Libraries/Lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.4.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="4555290_NCC_linkInfo.xml" --rom_model -o "4555290_NCC.out" <object modules> "../tm4c1237h6pz.cmd" "../Libraries/Lib/crc.lib" "../Libraries/Lib/lin_int.lib" "../Sup_Sm_Model/Libraries/Lib/crc.lib" "../Sup_Sm_Model/Libraries/Lib/lin_int.lib" -llibc.a -ldriverlib.lib
<Linking>
This does not happen with the version 17.6.0 STS of the compiler (or 15.X:X).
'Building target: 4555290_NCC.out'
'Invoking: ARM Linker'
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 -me -O2 --define=ccs="ccs" --define=PART_TM4C1237H6PZ --define=TARGET_IS_BLIZZARD_RB1 --define=__STDC_LIMIT_MACROS --define=_32_BIT_DOUBLE --float_operations_allowed=32 --gcc --diag_suppress=10190 --diag_warning=225 --diag_wrap=off --display_error_number --abi=eabi --check_misra="2.1,2.3,4,5.2,5.3,5.4,6.1,6.2,6.4,6.5,7,8.1,8.2,8.5,8.6,8.8,8.11,8.12,9" -z -m"4555290_NCC.map" --heap_size=2048 --stack_size=0 -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/lib" -i"C:/ti/TivaWare_C_Series-2.1.3.156/driverlib/ccs/Debug" -i"C:/Projects/BIC - 0580181 - Cosmogas/2 - Develop/5 - Firmware/4555290_NCC/Libraries/Lib" -i"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="4555290_NCC_linkInfo.xml" --rom_model -o "4555290_NCC.out" <object modules> "../tm4c1237h6pz.cmd" "../Libraries/Lib/crc.lib" "../Libraries/Lib/lin_int.lib" "../Sup_Sm_Model/Libraries/Lib/crc.lib" "../Sup_Sm_Model/Libraries/Lib/lin_int.lib" -llibc.a -ldriverlib.lib
<Linking>
'Finished building target: 4555290_NCC.out'
' '
"C:/ti/ccsv7/utils/tiobj2bin/tiobj2bin" "4555290_NCC.out" "4555290_NCC.bin" "C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armofd" "C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armhex" "C:/ti/ccsv7/utils/tiobj2bin/mkhex4bin"
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armdis" "4555290_NCC.out" "4555290_NCC.lst"
Disassembling 4555290_NCC.out into 4555290_NCC.lst
"C:/ti/ccsv7/tools/compiler/ti-cgt-arm_17.6.0.STS/bin/armnm" -o="4555290_NCC.sym" "4555290_NCC.out"
' '
**** Build Finished ****
Can you provide me with some info and tips to solve the issue?
By the way I would also like to use the linker to fill the stack with a specific pattern (say 0xFEFEFEFE). Is it possible?
For your reference, this is the linker command file
/******************************************************************************
*
* Default Linker Command file for the Texas Instruments TM4C1237H6PZ
*
* This is derived from revision 10691 of the TivaWare Library.
*
*****************************************************************************/
--retain=g_pfnVectors
#defineFLASH_START 0x00000000
#defineFLASH_SIZE 0x00040000
#defineFLASH_END (FLASH_START + FLASH_SIZE -1)
#defineRAM_START 0x20000000
#defineRAM_SIZE 0x00008000
#defineRAM_END (RAM_START + RAM_SIZE -1)
#defineROM_START 0x01000000
#defineROM_END 0x010087FF
#defineROM_SIZE (ROM_END - ROM_START + 1)
#defineVESTA_SIZE (0x00008000 - CRCDATA_SIZE)
#defineCRCDATA_SIZE (SIZE(CRCDATA)
MEMORY
{
CRCDATA (R) : origin = 0x3FFFC, length = 0x00000004, fill = 0xFFFFFFFF
FLASH (RX) : origin = FLASH_START, length = START(CRCDATA)-FLASH_START, fill = 0xFFFFFFFF
SRAM (RWX) : origin = RAM_START, length = 0x00007F00, vfill = 0x00000000
PERSISTENT (RW) : origin = 0x20007F00, length = 0x00000100
}
/* The following command line options are set as part of the CCS project. */
/* If you are building using the command line, or for some reason want to */
/* define them here, you can uncomment and modify these lines as needed. */
/* If you are using CCS for building, it is probably better to make any such */
/* modifications in your CCS project and leave this file alone. */
/* */
/* --heap_size=0 */
/* --stack_size=256 */
/* --library=rtsv7M4_T_le_eabi.lib */
/* Section allocation in memory */
SECTIONS
{
.intvecs: > 0x00000000
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.crcval1 : >CRCDATA
//.vtable : > 0x20000000
.stack : > RAM_START /* fill = 0xFEFEFEFE */
//.vtable : > SRAM
.sysmem: > SRAM (HIGH) { __SYSMEM_START = .; }
.data : > SRAM (HIGH)
.bss : > SRAM (HIGH)
.persistent : > PERSISTENT, type=NOINIT
}
__STACK_SIZE = __SYSMEM_START - RAM_START;
__XX = __SYSMEM_START;
__STACK_TOP = __SYSMEM_START - 0x08;
__STACK_END = __STACK_TOP + 0x04;
__CRCDATA_START = FLASH_END+1-CRCDATA_SIZE;
__ROM_START = ROM_START;
__ROM_END = ROM_END;
__ROM_SIZE = ROM_SIZE;
__CRCVAL1_START = START(CRCDATA);
__PERSISTENT_START = START(PERSISTENT);
__FLASH_START = START(FLASH);
__FLASH_SIZE = START(CRCDATA)-FLASH_START;
__FLASH_END = __FLASH_START + __FLASH_SIZE - 1;
__RAM_START = START(SRAM);
__RAM_SIZE = RAM_SIZE;
__RAM_END = __RAM_START + __RAM_SIZE - 1;