Part Number: TPS65217
We are testing a new lot of production boards that use the TPS65217C to power the AM3358BZCZ100, and on one of the boards, LDO3 has only 0.65 volts output instead of 1.8V (no apparent short on output; all other outputs are OK). However, the PGOOD pin is high, indicating that the regulator's output is in spec. What could cause this?