Part Number: LAUNCHXL-CC1350
Tool/software: Code Composer Studio
Hi,
I use ccs 7.1 and compiler TI v16.9.3.LTS.First I set the timestamp by Seconds_set(timestamp). Then I wanted to set local time eg gmtime (..). From the forum I learned that there is _tz structure that stores timezone data. The default values are:
TZ _tz =
{
-1, /* daylight */
21600, /* timezone */
"CST", /* tzname */
"DST", /* dstname */
};
gmtime(..) gives date according to timezone (UTC+6). But when I change the timezone to negative gmtime shows an error (for CST should be -21600 !). The source of gmtime.c has the condition:
_CODE_ACCESS struct tm *GMTIME(const TIMET *timer)
{
TIMET gtime = _tz.timezone; /* DIFFERENCE BETWEEN CURRENT TIME ZONE */
/* AND GMT IN SECONDS */
/*-----------------------------------------------------------------------*/
/* If we overflow time_t by adding the timezone, return NULL */
/*-----------------------------------------------------------------------*/
#if defined(_TIME64_IMPLEMENTATION)
if (*timer > INT64_MAX - gtime) return NULL;
#else
if (*timer > UINT32_MAX - gtime) return NULL;
#endif
if (timer) gtime += *timer;
return LOCALTIME(>ime);
}
When gtime < 0 there is overflow I think. How can I change this library? Is it true that DST(Daylight Saving Time) is not implemented?
JacekRz