Tool/software: TI C/C++ Compiler
My code composer is giving the following error when I try to build the program:
INTERNAL ERROR: C:\ti\ccsv7\tools\compiler\ti-cgt-arm_16.9.4.LTS\bin\armlnk.exe experienced an unhandled exception
This is caused by a defect in the TI Linker.
TI Customer Support may be able to suggest a workaround to avoid this.
Upgrading to the newest version of the compiler may fix this problem.
Contact TI in the E2E support forums at http://e2e.ti.com under
"Development Tools", "TI C/C++ Compiler". See the link titled
"Submitting an issue".
We need to see this ENTIRE error message and a complete, reproducable
test case including ALL of the command-line options.
Include all of the object files, libraries, and linker command files
used to link the program.
>> Compilation failure
makefile:190: recipe for target 'HerculesDev.out' failed
gmake[1]: *** [HerculeHerculesDev-master.zipsDev.out] Error 1
gmake: *** [all] Error 2
makefile:186: recipe for target 'all' failed
**** Build Finished ****