Part Number: MSP430-GCC-OPENSOURCE
Tool/software: TI C/C++ Compiler
There had been a question two years ago about the way to follow up / feedback to the open source MSP430 GCC fork //e2e.ti.com/support/development_tools/compiler/f/343/p/396532/1402922#1402922 but no news since then. I did not find a way to communicate with the maintainer w.r.t. their patch so I am using this forum. Please forward the following to Jozef Lawrynowicz:
In regard to this patch: patchwork.ozlabs.org/.../ that is included in the version of gcc that one can download from the TI site, it is my understanding that the file "devices.csv" is looked up in the "-I" and "-L" directories that where specified in the command line, but _not_ the include and library directories that are built in into compiler/toolchain. If my understanding is correct, may I suggest that builtin paths are also checked? Then the user can put the file into e.g ${PREFIX}/msp430-elf/include directory and save the effort of explicitly specifying the include directory in their Makefile.
Thank you,
Eugene