Tool/software: TI C/C++ Compiler
Hello,
I'm using C6x compiler with CCS project and I would like them to be portable. I have a problem with the "link order" property.
To have a portable CCS project, I only use environment variables.
Here below what I do :
1) I In the "File Search Path" property of the C6000 Linker, I add a --library => "${PATH}/file.cfg"
2) To link my project , I fill the "link order"property of my project => my cmd file has to be placed after the --library declared before.
I noticed then that the PATH variable has been interpreted that it is confirmed if I open and read the .cprojet file (we can see an absolute path in the listOptionValue).
The problem is that when I move my project in a different directory, the link command failed because the link order property has not been updated with the new path
Maybe someone could help me to resolve this problem ? thank in advance for your help.
Pat.