Part Number: MSP432P401R
Tool/software: TI C/C++ Compiler
Hello everybody:
I have a code question. It may be a silly question but I am a beginner so please have patience.
I have been working with the MSP430F5529 Launchpad for a couple of years and just purchased my new MSP432.
I noticed that the example code is a little bit different; for example to configure a port, instead of P1DIR |= BIT0;, it has P1->DIR |= BIT0;
If I enter as the first example, it will work fine.
I was just wondering if there is any benefit of the second example over the first example.
Is it faster or easier for the processor? or, Can I just continue to write the code as I did with the '5529?
Would really appreciate any comment.
Thanks!
Ralf