Part Number: OMAP3530
Tool/software: TI C/C++ Compiler
I'm having some trouble with the hex-file generation tools between versions of the compiler. I don't see anything in the documentation indicating that there are changes between these versions.
Somehow the base-address of the executable is being lost during translation.
I'm invoking the tool with
/ti/ccsv7/tools/compiler/ti-cgt-arm_18.1.1.LTS/bin/armhex.exe -map=st-app.map -a st-app.out -o st-app.hex -order MS -romwidth 32
If I build with 18.1.1.LTS, the first couple of lines of the hexfile look like:
$A0000,
00 40 2D E9 D1 6D 00 EB B7 70 00 EB 00 80 BD E8 00 00 72 87 00 00 80 00
(There is another line with a non-standard character to start the file. The A0000 address is *not* correct.
However if I run the 16.9.6 version of armhex.exe (same options) on the very same .bin file, I get:
$A84000000,
00 40 2D E9 D1 6D 00 EB B7 70 00 EB 00 80 BD E8 00 00 72 87 00 00 80 00
This is correct (or at least not obviously wrong).
Any thoughts?
John