Tool/software: Code Composer Studio
Hi Team,
I have a customer who is using an MSP430F67691 and running into a build problem. They are currently using CCS 7.4.0.00015. Please see the description below and thanks for the help in advance:
"There are multiple CCS projects involved, but the essence of the problem shows up in one project. It builds a relocatable output module. There is no main() in this project. When I look at the .map file generated by the linker, there are undefined references. Most of these get resolved when the .lib file is linked in the “final” project, but some (MPUCTL0, MPUSAM, MPUSEG, etc.) don’t. The unresolved references are to registers in the MSP430FR parts. Of course the part I’m using doesn’t have these registers. I can’t figure out why the build process is making reference to these non-existent registers."
Thanks again for the help and efforts.
Best,
Jerry