Tool/software: TI C/C++ Compiler
Support Path: /Tools & software/Help me with an issue/Embedded Product Development Tools/Code Composer Studio/CCS Desktop IDE/CCSv6 general issues/
Hello,
I had an issue with this before and got things working with CCS6, but now I'm doing a new project in CCS7(I doubt if CCS6 or 7 is the issue)
I'm frustrated trying to do something simple! I merely want to use names for individual output or input port pins. For Example: to set a port bit to 1, I'd like to just say RED_LED=1;
Please tell me the simplest way to do this, either a defined structure/macro or whatever.
Instead of using P1OUT ^= BIT0;
If I
#define RED_LED= B8_0(&P0OUT)
#define B8_0(x) (((volatile struct bits8 *) (x)) ->b0)
i get an (error #29 expression expected)
Very Much Appreciated
Thank You