This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TMS320F28377S: MISRA-C:2004 12.6/A

Part Number: TMS320F28377S

Tool/software: TI C/C++ Compiler

Wrong MISRA-C :2004 warning:

../main.c", line 73: warning #1483-D: (MISRA-C:2004 12.6/A) Expressions that are effectively Boolean should not be used in operations with expressions that are not effectively Boolean

Code for reproducing:

typedef unsigned int u16_t;

void testme(u16_t u16_tv);

typedef struct {

u16_t au16_test[6];

u16_t u16_tw;

} ST_Test;

ST_Test mast_test[3];

void testme(u16_t u16_tv)

{

mast_test[0].u16_tw = u16_tv + 0u;

mast_test[0].u16_tw = u16_tv;

}

/**

* Application entry point

*/

void main(void)

{

testme(23u);

}

Full build output:

**** Build of configuration Debug for project boot ****

"D:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 4 all -O

Building file: "../main.c"

Invoking: C2000 Compiler

"D:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 -O0 --opt_for_speed=2 --include_path="C:/Users/L029453/DSPbase2/ti_boot" --advice:performance=all -g --c89 --relaxed_ansi --diag_warning=225 --diag_wrap=off --display_error_number -k --asm_listing --check_misra="all,-1.1,-2.2,-5.7,-11.3,-17.4" --preproc_with_compile --preproc_dependency="main.d_raw" "../main.c"

"../main.c", line 73: warning #1483-D: (MISRA-C:2004 12.6/A) Expressions that are effectively Boolean should not be used in operations with expressions that are not effectively Boolean

Finished building: "../main.c"

Building target: "boot.out"

Invoking: C2000 Linker

"D:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.1.LTS/bin/cl2000" -v28 -ml -mt --cla_support=cla1 --float_support=fpu32 --tmu_support=tmu0 --vcu_support=vcu2 -O0 --opt_for_speed=2 --advice:performance=all -g --c89 --relaxed_ansi --diag_warning=225 --diag_wrap=off --display_error_number -k --asm_listing --check_misra="all,-1.1,-2.2,-5.7,-11.3,-17.4" -z -m"boot.map" --stack_size=0x200 --warn_sections --reread_libs --diag_wrap=off --display_error_number --xml_link_info="boot_linkInfo.xml" --rom_model -o "boot.out" "./adc.obj" "./bootF2837x.obj" "./devsys.obj" "./flash.obj" "./gpio.obj" "./main.obj" "./ramcheck.obj" "./wdog.obj" "../linkerF2837x.cmd"

<Linking>

Finished building target: "boot.out"