Tool/software: TI C/C++ Compiler
when compiled with TI compiler 16.9.6 in -Os mode the mbedTLS SHA-512 implementation produces incorrect results.
test code below is the excerpt that misbehaves - in particular, it looks like 64-bit shifts by more than 32 positions are not handled correctly.
#define GET_UINT64_BE(n,b,i) \
{ \
(n) = ( (uint64_t) (b)[(i) ] << 56 ) \
| ( (uint64_t) (b)[(i) + 1] << 48 ) \
| ( (uint64_t) (b)[(i) + 2] << 40 ) \
| ( (uint64_t) (b)[(i) + 3] << 32 ) \
| ( (uint64_t) (b)[(i) + 4] << 24 ) \
| ( (uint64_t) (b)[(i) + 5] << 16 ) \
| ( (uint64_t) (b)[(i) + 6] << 8 ) \
| ( (uint64_t) (b)[(i) + 7] ); \
}
static void test64(void) {
uint64_t w[2] = {0, 0};
int i;
static const uint8_t td[16] = {
0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07,
0x08, 0x09, 0x0a, 0x0b, 0x0c, 0x0d, 0x0e, 0x0f
};
for (i = 0; i < 2; i++) {
GET_UINT64_BE(w[i], td, i << 3);
}
for (i = 0; i < sizeof(w); i++) {
printf("%02x ", ((uint8_t *) w)[i]);
}
printf("\n");
}
when run, it produces the following output:
07 06 05 04 03 00 00 00 0f 0e 0d 0c 0b 00 00 00
note that top 3 bytes in the uint64_ts are zeroes, so it looks like shifts by 40, 48 and 56 result in 0 in the | operator above.
this is the assembler code generated by the compiler:
0103eaf4 <test64>:
103eaf4: b5f0 push {r4, r5, r6, r7, lr}
103eaf6: 2100 movs r1, #0
103eaf8: 2210 movs r2, #16
103eafa: f1ad 0d14 sub.w sp, sp, #20
103eafe: 4668 mov r0, sp
103eb00: f005 fc3e bl 1044380 <memset>
103eb04: 4c24 ldr r4, [pc, #144] ; (103eb98 <test64+0xa4>)
103eb06: 466d mov r5, sp
103eb08: 2300 movs r3, #0
103eb0a: 2702 movs r7, #2
103eb0c: 78e6 ldrb r6, [r4, #3]
103eb0e: 78a0 ldrb r0, [r4, #2]
103eb10: 17f1 asrs r1, r6, #31
103eb12: 4318 orrs r0, r3
103eb14: 0202 lsls r2, r0, #8
103eb16: ea46 0003 orr.w r0, r6, r3
103eb1a: 4311 orrs r1, r2
103eb1c: 0e02 lsrs r2, r0, #24
103eb1e: 0206 lsls r6, r0, #8
103eb20: 7920 ldrb r0, [r4, #4]
103eb22: 0209 lsls r1, r1, #8
103eb24: 4311 orrs r1, r2
103eb26: 17c2 asrs r2, r0, #31
103eb28: 430a orrs r2, r1
103eb2a: 4330 orrs r0, r6
103eb2c: 0211 lsls r1, r2, #8
103eb2e: 0206 lsls r6, r0, #8
103eb30: 0e02 lsrs r2, r0, #24
103eb32: 7960 ldrb r0, [r4, #5]
103eb34: 4311 orrs r1, r2
103eb36: 17c2 asrs r2, r0, #31
103eb38: 430a orrs r2, r1
103eb3a: 4330 orrs r0, r6
103eb3c: 0211 lsls r1, r2, #8
103eb3e: 0206 lsls r6, r0, #8
103eb40: 0e02 lsrs r2, r0, #24
103eb42: 79a0 ldrb r0, [r4, #6]
103eb44: 4311 orrs r1, r2
103eb46: 17c2 asrs r2, r0, #31
103eb48: 430a orrs r2, r1
103eb4a: 4330 orrs r0, r6
103eb4c: 0211 lsls r1, r2, #8
103eb4e: 0206 lsls r6, r0, #8
103eb50: 0e02 lsrs r2, r0, #24
103eb52: 79e0 ldrb r0, [r4, #7]
103eb54: 1e7f subs r7, r7, #1
103eb56: ea41 0102 orr.w r1, r1, r2
103eb5a: ea4f 72e0 mov.w r2, r0, asr #31
103eb5e: f104 0408 add.w r4, r4, #8
103eb62: ea42 0101 orr.w r1, r2, r1
103eb66: ea40 0006 orr.w r0, r0, r6
103eb6a: c503 stmia r5!, {r0, r1}
103eb6c: d1ce bne.n 103eb0c <test64+0x18>
103eb6e: 2410 movs r4, #16
103eb70: 466d mov r5, sp
103eb72: f815 1b01 ldrb.w r1, [r5], #1
103eb76: a005 add r0, pc, #20 ; (adr r0, 103eb8c <test64+0x98>)
103eb78: f006 ffd0 bl 1045b1c <printf>
103eb7c: 1e64 subs r4, r4, #1
103eb7e: d1f8 bne.n 103eb72 <test64+0x7e>
103eb80: a004 add r0, pc, #16 ; (adr r0, 103eb94 <test64+0xa0>)
103eb82: f006 ffcb bl 1045b1c <printf>
103eb86: b005 add sp, #20
103eb88: bdf0 pop {r4, r5, r6, r7, pc}
103eb8a: 46c0 nop ; (mov r8, r8)
103eb8c: 78323025 .word 0x78323025
103eb90: 46c00020 .word 0x46c00020
103eb94: 46c0000a .word 0x46c0000a
103eb98: 01059282 .word 0x01059282