Other Parts Discussed in Thread: C2000WARE
Tool/software: TI C/C++ Compiler
c2000 compiler 18.1.1.LTS and C2000Ware_1_00_04_00
Using blinky example for CPU1 for F2837xD control card
In F2837xD_SysCtrl.c
If I have MISRA checking enabled for only section 12.6 in this SysCtrl file, I get some lines that violate 12.6. Some are actually violating 12.6, and some I think are incorrectly interpreted as violating 12.6.
Specifically,
// line 630 ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = divsel; // line 851 WdRegs.WDCR.all = WDCR; // line 882 ClkCfgRegs.SYSCLKDIVSEL.bit.PLLSYSCLKDIV = divsel;
#1483-D (MISRA-C:2004 12.6/A) Expressions that are effectively Boolean should not be used in operations with expressions that are not effectively Boolean
where it seems nothing boolean is going on here.