Part Number: TMS320F28377S
Tool/software: TI C/C++ Compiler
Hi TI
I recently wanted to assign some bits to a 32 bit unsigned long value this way and saw a strange behavior of the optimizer.
This code is reduced to show what I mean:
volatile char myGlobalVolatileCharIsOne = 1;
unsigned long myFunction(void)
{
unsigned long Result = 0UL;
myGlobalVolatileCharIsOne = 1;
Result |= ((myGlobalVolatileCharIsOne ? 1UL : 0UL) << 1);
Result |= ((myGlobalVolatileCharIsOne ? 1UL : 0UL) << 16);
return Result;
}
I did expect Result = 0x00010002.
With -Ooff I get Result = 0x00010002
With -O3 I get Result = 0x00000002
It seems somewhere to be related to the left shift. If I write the expression this way is works as expected:
Result |= (myGlobalVolatileCharIsOne ? 0x00010000UL : 0UL);
This way is also ok:
Result |= (myGlobalVolatileCharIsOne ? (1UL<<16) : 0UL);
CGT 16.9.8 and CGT 18.1.3
Best regards
Roger