Tool/software: TI C/C++ Compiler
Dear Compiler Experts,
I have the following line of code inside a function:
uint8_t wr_buf[8] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};
The corresponding disassembly is:
475 uint8_t wr_buf[8] = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};
$C$L89:
0000037e: 4991 ldr r1, [pc, #0x244]
00000380: 680A ldr r2, [r1]
00000382: A802 add r0, sp, #8
00000384: 6002 str r2, [r0]
00000386: 6849 ldr r1, [r1, #4]
00000388: 6041 str r1, [r0, #4]
At the second ldr I get an exception 3.
What is wrong with the code? Why doesn't the compiler complain about?
When using the following code it works fine:
uint8_t wr_buf[8];
uint32_t idx;
for (idx=0; idx<8; idx++) {
wr_buf[idx] = 0xFF;
}