Hello,
I have recently purchased the GPIO to USB EVM Adapter and am having trouble configuring the 8 GPIO signals as inputs using the provided "USB Interface Adapter GUI-v1.10" application. Toggling the different checkboxes in the GPIO group box section and hitting Read/Write either changes the signals from an output driving high or an output driving low. I have yet to get the signals to tri-state as an input. What do I need to do to configure the 8 pins as inputs?
Also, any help on using the “USB Adapter Driver.dll” library to configure the device would be appreciated too. Are the following routines “gpioReadWrite()”, “setControl ()”, or “getControl()” correct for setting the pins as inputs an reading the values?.
Sincerely,
Matthew