Hello everyone
I want to design a Sallen & Key Butterworth filter with frequency range 20Hz to 500Hz, but im not sure if filling in the right parameters. Could you all please give me some guidance.. I entered the following parameters into filterPro:
Gain A0 = 1 V/V = 0dB
Centre Frequency F0 = 260Hz ; Because (500Hz-20Hz)/2 + 20 = 260
Allowable Passband Ripple Rp = 0dB (Butterworth Characteristics)
Passband Bandwidth BWp = 480Hz; Because 500Hz - 20Hz = 480
Stopband Bandwidth = 10000 (Im not sure how to select stopband bandwidth, I just keep trying 10,100,1000,10000,1000000..
Stopband Attenuation = -45 degrees
This is the band pass filter generated by filterPro. Is it really a band pass filter with frequency range 20Hz to 500Hz.
Thanks!