Hello Guys,
Good day.
Datasheet suggests that for illumination between 700nm to 2500nm, the max power is thermally limited. What does this mean? If a customer want to use a laser of 1064nm on the DMD, and the power would be something like 40W/cm^2. Is that okay? Is there an absorption spectrum for this device anywhere?
Thanks and regards,
Art