Other Parts Discussed in Thread: DLPC3436
We have been able to successfully connect the evaluation module via a Raspberry Pi 3 a+ and have video play but have not been successful with connecting a Raspberry Pi Zero W. Do to environmental restrictions, it is ideal that we are able to use the Raspberry Pi Zero W.
When hooking up the Raspberry Pi Zero W and DLP evaluation module, the Raspberry Pi initially freezes and reboots itself. Once it has rebooted, the DLP evaluation module with first go to the splash screen then turn grey as the connection is being made. What happens with the Raspberry Pi 3 a+ is that once the connection is done, the desktop is displayed. This is not the case for the Zero W. Instead the projector turns off.
I then will try to connect with the DLP evaluation module by typing in the command python3 init_parallel_mode.py and get an error, which you can see via the attached image.
Please let me know if there is a way around this or if the Raspberry Pi Zero W is not compatible with this DLP evaluation module.