Dear TI,
I successfully connected DLPC9000 evaluation board to my computer and try to control it through GUI. I can see green 'connected' on the GUI and lights on the evaluation board on indicating chips are working. This is not a new part and I bought it several months ago. However, since the beginning, I cannot stand by the DMD through GUI, nor could I read status from DMD(e.g. on system settings panel, there are 'GET LED Control', 'GET DMD Park'). When I tried so, an error occurred.
For standby, it says "Unable to get StandbyDelaySec Error: Invalid command number: 0x1A25"
For DMD park get, it says "Unable to Read DMD park status Error: Invalid command number: 0x609"
However, when I connected DMD to an official power supply, it starts to scan over its pre-stored patterns automatically. I could also use pattern on-the-fly mode, including uploading LUT, start/stop sequence.
Could you please tell me what's the problem? Thank you!