This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR4710EVM-G2: EVM specs and measurements for the housing

Part Number: DLPDLCR4710EVM-G2
Other Parts Discussed in Thread: DLP4710,

Hi Team, 

May I ask for help? Below is the initial concern of our customer:
"I would like the data sheet for the DMD mount that houses the DLP4710 DMD in this EVM. We are attempting to build a custom mount or make changes to the existing housing. A datasheet for the EVM would be helpful with specs and measurements for the housing. To be clear it is the matte light gray metal housing the holds the DMD, the output lenses and the chip that interfaces with the dmd. Please find attached an image of the part we are interested in, the red circle indicated the specific region of the part we need the details for. The material properties of the mount would also be helpful."

Image is shown below:


Then as an initial solution, I ask the customer to refer to the link below for the CAD files of DLPDLCR4710EVM-G2.

Link: www.ti.com/.../TIDA-01226

But customer responded as below:

"Im not sure if the model given represents the actual part? here are some photos and screenshots?

The pins in the body that hold the dmd are not present in the CAD model. Is there a more updated version?"





May we ask why is there a difference? Is the CAD files in the link not updated for DLPDLCR4710EVM-G2
We would really appreciate if you can provide us the measurements/drawing in pdf or cad file.

We will wait for your response and thank you so much in advance.

Regards,
 
Gerald