Other Parts Discussed in Thread: DLP4710LC,
Hello,
i am currently using my DLP4710LC and for the project, i need to tear down the device and unplug the LEDs. Before i used DLP4710G2 in my desired configuration, it works clearly that i dont need to plugin the LEDs and it can do output with HDMI. But i tried similar way to the DLP4710LC which i upload the firmware with desired batch file, it is not working. It always has a small current of all LEDs and is not totally switch off as in batch file i gave # 0x52 - Rgb Led Enable w 36 52 00
It seems 4710LC is always checking the LEDs and power them up when boost up
Is there any way to disable and unplug the LEDs and even disable the checking process of LEDs directly from the starting for 4710LC?
It will much helpfull if any solution given
Best regards,
Haoran Wang