This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP4710EVM-LC: dlp4710LC

Part Number: DLP4710EVM-LC
Other Parts Discussed in Thread: DLPC3479

Hi TI 

https://e2e.ti.com/support/dlp-products-group/dlp/f/dlp-products-forum/1016077/dlp4710evm-lc-disable-and-unplug-all-leds-from-the-evm?tisearch=e2e-sitesearch&keymatch=DLP4710EVM-LC#

I am an engineer, from Wintech Inc Which is a TI's Third party, and mainly responsible for DLP Engine development

Encountered a problem when developing 4710LC equipment

How can i set  Led current 0 mA  by using TI's GUI?

The minimum is 1423,

I can not set 0

Austin  shared Composer Project with me ,DLPC3479_Software_Release_v7.0.1.zip

The minimum is 51 in the project config

How can I set LED current from 0 to 1023?

and

the led is black when the current setting is 0

like this

out application is 3D printer

Thanks very much

Best Regards

Jia

  • Hi Jia,

    We set the minimum LED current above zero because of the inherent non-linearities of LEDs at low current. this lower limit is to "protect people from themselves". the image quality may become very bad.

    It is possible to remove this limit, and I have a composer project i can share with you. However you will need to adjust the current in DLP Composer under Projector Control -> Illumination -> RGB LED current. This is because the GUI software has a hard coded limit. 

    I sent you a friend request we can continue to discuss in private message.

    Regards,

    Arthur Brown