Other Parts Discussed in Thread: DLPC3479
Hi TI
I am an engineer, from Wintech Inc Which is a TI's Third party, and mainly responsible for DLP Engine development
Encountered a problem when developing 4710LC equipment
How can i set Led current 0 mA by using TI's GUI?
The minimum is 1423,
I can not set 0
Austin shared Composer Project with me ,DLPC3479_Software_Release_v7.0.1.zip
The minimum is 51 in the project config
How can I set LED current from 0 to 1023?
and
the led is black when the current setting is 0
like this
out application is 3D printer
Thanks very much
Best Regards
Jia