Other Parts Discussed in Thread: DLPC3439, DLP4710, DLPC3479
Hi,
We use DLPA3005 and DLPC3439 In our previous system. Out system has only one blue channal supporting one LED drive( VF=3.6V). It works fine. Now we want to use two LED in series(VF=7.35V), it does not works. When I enable the LED output, the DLPA3005 would detect some fault and kill the voltage supply to protect itself. So how do I adjust the output voltage(VLED) window to support two LED in series?
Thanks.