Other Parts Discussed in Thread: DLPC3436
Hi TI,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI,
Hide-san,
Does the communication error persist if you read the register multiple times? Sometimes the error may fire a single time during boot.
Furthermore, have you been able to get a video output from the Raspberry Pi (to ensure that you have the EVM configured properly)? There are Python sample scripts which configure the EVM for RGB666 operation available on the EVM tool folder. If you are having trouble with the ITE6801 it may be a good idea to start there and work your way towards the 6801.
The DLPC3436 chipset (which is what the EVM uses) supports the ITE6801 so you should be able to get both modes of operation working with the right settings.
https://www.ti.com/tool/DLPDLCR230NPEVM
Regards,
Philippe Dollo
Hi Philippe,
Long time no see!
Yes, the issue persists multiple times.
As you suggested, I will check if the EVM is configured properly with RaspberryPi.
The longest way round is the nearest way home.
Having heard that the DLPC3436 supports the ITE6801 is good information and helpful.
Thank you very much for your support.