Other Parts Discussed in Thread: DLP4500, , DLPC3478
Hello,
My customer is asking the same issue as below.
Is the DLPC350/DLP4500 fixed this issue on the latest fw version?
Regards,
Uryyy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Uryyy,
I'll notify the team so that we can verify within the next few days if this issue has been resolved. However, I would note that these two chipsets are unique so the issue presented may not translate well to the DLPC350 chipset.
Regards,
Philippe
Uryyy,
It would appear that this issue was examined at a granular level specific to the DLPC3478 chipset. As such, if there is a solution that is applicable to the DLPC350 (and if the issue translates equally to this platform) then it would not have been implemented at this time.
If you are seeing a similar issue, the team will need additional details to be able to investigate:
> Are you using external/internal pattern streaming modes? Can you describe your configuration in more detail?
> Do you see this issue across multiple EVM units? What about across multiple firmware versions?
> What GUI version are you using?
Best Regards,
Philippe
Hello,
Since there has been no activity for 22 days, I will be closing this thread.
Thank you,
Chris