Part Number: DLPDLCR2000EVM
Hello,
I am using the DLP® LightCrafter Display 2000 Evaluation Module (EVM) and its DMD. I am exporting the DMD's display. For that, I use the following line code:
export DISPLAY=:0
It works when I type this command and press enter. However, I need to have that on a file code to run it instead of writing the same line every time I need to use the DMD. I wrote the following code file and some variations of it. The command to turn off the LED works well, but turning on the Display does not work.
#!/bin/bash
#turn off LED
i2cset -y 2 0x1b 0x16 0x00 0x00 0x00 0x00 i
#turn on Display
export DISPLAY=:0
Please, how could I solve this issue?
Thank you,
Thaisa