Other Parts Discussed in Thread: DLP4710EVM-LC,
Hi,
We are currently using the DLPDLCR4710EVM-G2 and DLP4710EVM-LC for some experiments which need to control the intensity of the light. We use the optical power and energy meter console from THORLABS to examine the optical power, and found that both products have some defects with the continuity of the light intensity. We have confirmed the defects also by the luxmeter and the Basler camera.
The DLPDLC GUI setting is as following:
We give the DLP a homo intensity picture which is a 8-bit one to get the optical power. Here's the DLPDLCR4710EVM-G2 data. The first column refers to the 8-bit blue channel. The second column refers to the radiometric we get from the optical meter.
"Gray Scale" "Radiometric(W/m^2,470nm,raw)" 0 0.001 1 0.001 2 0.001 3 0.001 4 0.001 5 0.002 6 0.002 7 0.002 8 0.002 9 0.002 10 0.002 11 0.002 12 0.003 13 0.003 14 0.003 15 0.003 16 0.004 17 0.004 18 0.004 19 0.005 20 0.005 21 0.005 22 0.006 23 0.006 24 0.007 25 0.007 26 0.008 27 0.008 28 0.009 29 0.009 30 0.01 31 0.011 32 0.011 33 0.012 34 0.013 35 0.013 36 0.014 37 0.014 38 0.015 39 0.016 40 0.017 41 0.018 42 0.018 43 0.019 44 0.021 45 0.022 46 0.023 47 0.024 48 0.025 49 0.026 50 0.027 51 0.028 52 0.029 53 0.03 54 0.032 55 0.033 56 0.034 57 0.035 58 0.036 59 0.038 60 0.039 61 0.041 62 0.042 63 0.044 64 0.045 65 0.047 66 0.048 67 0.05 68 0.051 69 0.053 70 0.055 71 0.056 72 0.058 73 0.059 74 0.061 75 0.063 76 0.065 77 0.066 78 0.068 79 0.07 80 0.072 81 0.074 82 0.076 83 0.078 84 0.08 85 0.082 86 0.084 87 0.086 88 0.089 89 0.091 90 0.093 91 0.096 92 0.098 93 0.1 94 0.103 95 0.105 96 0.107 97 0.11 98 0.112 99 0.114 100 0.117 101 0.119 102 0.122 103 0.124 104 0.127 105 0.13 106 0.132 107 0.136 108 0.138 109 0.141 110 0.144 111 0.147 112 0.15 113 0.153 114 0.155 115 0.156 116 0.159 117 0.162 118 0.165 119 0.168 120 0.171 121 0.174 122 0.177 123 0.181 124 0.184 125 0.187 126 0.191 127 0.194 128 0.198 129 0.201 130 0.205 131 0.208 132 0.212 133 0.216 134 0.219 135 0.223 136 0.226 137 0.23 138 0.234 139 0.238 140 0.242 141 0.246 142 0.249 143 0.253 144 0.257 145 0.26 146 0.264 147 0.267 148 0.271 149 0.275 150 0.279 151 0.284 152 0.288 153 0.292 154 0.296 155 0.302 156 0.307 157 0.309 158 0.313 159 0.317 160 0.321 161 0.331 162 0.337 163 0.335 164 0.34 165 0.344 166 0.349 167 0.353 168 0.363 169 0.366 170 0.367 171 0.371 172 0.376 173 0.381 174 0.385 175 0.39 176 0.395 177 0.4 178 0.405 179 0.411 180 0.415 181 0.42 182 0.425 183 0.43 184 0.435 185 0.44 186 0.445 187 0.45 188 0.442 189 0.442 190 0.45 191 0.454 192 0.458 193 0.463 194 0.468 195 0.475 196 0.48 197 0.486 198 0.491 199 0.5 200 0.507 201 0.512 202 0.517 203 0.522 204 0.528 205 0.534 206 0.539 207 0.545 208 0.551 209 0.558 210 0.563 211 0.569 212 0.575 213 0.58 214 0.586 215 0.592 216 0.6 217 0.605 218 0.609 219 0.615 220 0.621 221 0.627 222 0.633 223 0.639 224 0.647 225 0.649 226 0.647 227 0.65 228 0.654 229 0.66 230 0.668 231 0.676 232 0.682 233 0.691 234 0.702 235 0.708 236 0.714 237 0.721 238 0.727 239 0.733 240 0.74 241 0.746 242 0.752 243 0.756 244 0.762 245 0.769 246 0.775 247 0.783 248 0.789 249 0.794 250 0.799 251 0.805 252 0.812 253 0.819 254 0.826 255 0.826
When the input gray scale meets about 185, there's a defect.
The other product DLP4710EVM-LC has a defect at about 177.
We are confused that whether we have a mistake in the DLP setting or there's other possible problems during the experiments.
Any hints would be appreciated.
Best Regards!