Other Parts Discussed in Thread: DLPA3005
For our structured light application we require a higher light output from the DLP4710EVM-LC module. From my understanding currently the blue LED is a Osram LE CG P1A 3.35V 16A module. We are planning on replacing this module with the more powerful LE B P2MQ 14V 12A. Looking at the schematics and datasheet, it seems that the dlpa3005 and power FETs would support this voltage / current range.
I would have two questions regarding feasibility of this modification:
- In the datasheet of the dlpa3005 it is written that V_LED_ANODE can be up to 6.2V, yet in some threads in this forum it was mentioned that V_LED_ANODE can be up to 0.85*V_IN (in this case 16.15V). Can you confirm that this is the case?
- The startup current seems to be fixed at 10A, is there a way to modify this value (make it lower) and make it persistent?
Thank you very much for your support!