Hi,
I used to work with the discovery 4100 explorer on an old workstation, where it worked just fine.
When I try to install it on a new computer I get the following error message during installation:
Than the installation terminates with the following message:
"Error executing post installation script
regsvr32
\Program ended with an error exit code"
When I tried to run "C:\Windows\SysWOW64> regsvr32 DDC4100.ocx" in the CMD window as suggested in this thread I got the following:
I would appreciate any help on this.
Thanks,
Ronen.