Other Parts Discussed in Thread: DLPC900
Hello Guys,
Good day.
Our customer is using the DLP LC 6500 in conjunction with a camera acquire images of various phantoms. The issue he'd been running into is that he can't seem to set the projector exposure above 11 seconds. At 11 seconds, the projector's exposure is fine, at 12 seconds it is around 1 second, at 15 seconds it is about 4 seconds, and when set at 90 seconds, the exposure seen is around 7 seconds. He was wondering why this issue was arising.
He was