That is, before the DMD is connected to the power supply and the data line, the welcome interface can be displayed. After using for a period of time, the DMD does not respond after the connection is connected or the DMD does not respond when the connection board is moved, but the GUI interface shows that the connection is normal and the green light is on. , But the DMD device has no response, it will work for a while, it will not work for a while, is it because of poor contact or is there any solution, whether it needs to be repaired, look forward to your reply, thank you