This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP3010LC: How to transfer out the footprintof DLP3010 to use?

Part Number: DLP3010LC
Other Parts Discussed in Thread: DLP3010, DLP3010EVM-LC

Hello, I would like to ask how the package pads of the general DLP3010 are connected and used? Should I use a board or a connector to transfer it out?
If I use a connector to switch it out, is there a recommended manufacturer and model? Because the pitch is 0.7424mm, which is too uncommon, I asked a few connector brands and didn't have it.

  • Sun,

    Welcome to the E2E forums and thanks for your interest in our DLP technology. 

    There are multiple ways to connect the DMD to a board. Typically, this is done with an interconnect like the one you shared above, though a direct board to board connector is sometimes used with certain DMDs. Are you looking to design your own optical engine or fixture?

    Regards,

    Philippe

  • Yes, we plan to design our own optical machine. We plan to use contacts to interconnect the connectors, but we can't find a suitable one because of the special spacing. Please help recommend suitable manufacturers and models, because we have not found suitable ones for mainstream manufacturers. thanks

  • Hello Sun,

    Contacting the optical module manufacturer of DLP3010EVM-LC might help you in addressing your query. You can refer to the following page to find contact information of the OMM (https://www.ti.com/tool/DLP-OMM-SEARCH) 

    Regards,

    Mayank