This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP500YX: Array Size is 2048x1080 or 2048x1200

Part Number: DLP500YX
Other Parts Discussed in Thread: DLPLCR50XEVM

Hi TI Expert:

From DLP500YX datahsheet,  the array size is 2048x1200. But in the explanation, it write 2048x1080. Is it working in 2048x1080 or 2048x1200?

And also the EVM is 2048x1080 from ti web:

//////////////////////////////////////////// 

EVALUATION BOARD

DLP® 0.50-inch, 2048x1080 array, S410 digital micromirror device (DMD) evaluation module

DLPLCR50XEVM
///////////////////////////////////////////////
 
I just comfused, which array size is correct or I had misunderstanding?