Other Parts Discussed in Thread: DLPC900
Hi E2E,
Our customer needs assistance with a DLP6500 device using a DLPC900 evaluation module. They have been attempting to eliminate a switching noise that comes from the DMD device jittering the mirrors every 105us to prevent the mirrors from getting stuck. This is the exact time scale they want for the patterns, so the noise is extremely loud and drowns out there measurements. Our customer have attempted to manually use commands on page 56 of the DLP Programmer's Guide to make sure the patterns don't wipe in that time, but using an external trigger doesn't cause any patterns to show up for them.
They are using a frequency generator to input the external trigger to control the patterns, while the DMD is ordered to not clear a pattern after exposure and instead wait for a trigger. This doesn't work as intended, but the process does work if they don't include the external trigger, so they're at a loss on how to proceed.
Thank you in advance for your help.
Regards,
Carlo