This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPDLCR2010EVM:Related quality issues that cannot be controlled by DLPDLCR2010EVM

Part Number: DLPDLCR2010EVM


I have used this DLPDLCR2010EVM for a period of time, and it still works normally at first, but suddenly there are some problems that make it unable to use normally. At present, DLPDLCR2010EVM can normally switch and project the startup screen, but other functions are basically unavailable, such as the function buttons on the board. Unable to realize the change of the control screen, and the display content cannot be projected when the HDMI interface is inserted. The screen is always the boot screen, and no program or hardware has been modified during use.