Other Parts Discussed in Thread: DLP5530-Q1
Hello Team,
Currently we are trying to use OPENLDI as external source with 1152 x 576 resolution on DLP5530. Our setup is
Embedded Platform -> 927 -> 928->OPENLDI->DLP5530.
But it is always throws source error 671.(Source Error External source Open LDI port pixel clock frequency is not within the allowable).
We have identified the Timing for Supported Source Resolutions( and following the same Page 11 of DLP5530PGUQ1EVM Evaluation Module User's Guide ).
Also, in the flash data summary, we have seen External video configuration selected for Parallel port, not for OPENLDI port. Please find the attached image for your reference.
Do we need to change flash data configuration to support OPENLDI output or is there any other suggestions to get the OPENLDI port?
Please help to suggest.
Thanks,
Sundar