Hello,
I'm using a DLP3010 projector and trying to switching between different pattern sets during the runtime.
For example: I have two pattern groups A and B for different features,
Group A contains 2 pattern set, the number of patterns in each set is 6 and 6.
Group B contains 2 pattern set, the number of patterns in each set is 6 and 6.
I use Group A as the default pattern order table when I program the flash using 3010 GUI.
In my code, I use DLPC34XX_DUAL_WritePatternOrderTableEntry to load the two pattern sets in group A and B during runtime.
I found that sometimes the projected patterns will be incorrect if I switch patterns from one group to another. After this issue happens, I immediately use "run once" on 3010 GUI, the patterns are still not correct. However, if I do "run once" a few more times, the patterns will be correct. And this issue happens again if I switch patterns again in my code.
I was wondering if it's possible to switch patterns during runtime by using API and how to properly do that.
Thanks,
Xinran