Hello,
My coworker purchased a DLPRC410EVM for a research project. I purchased a 5V, 6amp power supply. I followed the directions on the manual precisely to turn it on, but nothing would power. No LEDs were triggered, even after inserting the power cable, attached the flex cable to DMD, and turning on the power switch. I cannot connect to the board either (since it does not turn on). Out of frustration, I purchased a used control board from a 3rd party and was able to turn it on and connect properly.
Is there anything that could be done to fix this, or do I need a new board?