Hello,
In the DLPC410 datasheet this signal is stated as active high, meaning, once the DLPR410 finished to load it will go high (page 14 in the DS)
but later on on page 61 (section 9.3 - Initialization Setup) it is stated that it is de-asserted:
9.3 Initialization Setup
9.3.1 Debugging Guidelines
Prior to checking the DLPC410 output signals, make sure the reference clock to the DLPC410 is running at 50MHz.
Check that DONE_DDC (pin K10) signal is asserted and ECP2_Finished is de-asserted indicating the DLPR410 PROM has
correctly programmed the DLPC410 Controller and the DLPC410 is running.
which is the correct functionality?