Other Parts Discussed in Thread: DLPC350
Hi,
We have been using DLPC350 firmware v3.1.0 with the DLP4500FQE for many years and it has been working well.
(The firmware we use on the DLPC350 is based on DLPR350PROM_v3.1.0.bin with out custom patterns in it. Firmware was build using LightCrafter GUI v3.1.0)
We have recently had to upgrade the mirror to DLP4500AFQE, on recommendation of TI. (NOTE that we are still using the DLPC350)
Can you confirm that the same firmware will work with this part?
i.e. can you confirm that we can continue using the same firmware image for the DLPC350 as before?
Also, could you please provide a link to a changelog detailing the differences between the 3.1.0 firmware, and the latest v4.4? Would it be worth us upgrading anyway if there are any bugfixes in that firmware?
Many thanks,
Oliver.