Other Parts Discussed in Thread: DLPC410, , DLP9500, DLP500YX, DLP300S
Hi Team,
May I ask for help? Our customer have a concern as shown below:
" I want to customize two light projector, here ask for your assistance. I am looking for DMD chip with 365nm output DMD, and the 455nm output DMD. The DMD is better have the resolution 1080p or the 2k. can you also give the this two options in consideration and give me the specification comparation, and the price as well. The DMD chips should also have the controller board."
I am now checking DLP9500UV and DLPC410 for the 365nm output DMD. Can you confirm if this is a fit solution?
As for 455nm output DMD, can you please advise of what device would fit and a controller for it? Thank you so much.
Kind regards,
Gerald