This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLPNIRSCANEVM not displaying the GUI when 192.168.0.10 is entered

Other Parts Discussed in Thread: DLPNIRSCANEVM

I connected my DLPNIRSCANEVM to connector 6 and also 14. Neither result in the ability to access IP 192.168.0.10.

I attempted to load driver for the COM Port but Windows10 says it has the best driver already.

I turned off the Windows10 automatic driver loading options and I still don't see the device with anything other than C:\WINDOWS\system\DRIVERS\usbser.sys

Is there a 64bit driver for the DLPNIRSCANEVM ?